This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 265
Part Number: BQ51010B
I want to charge a small LiPo battery of 3,7V. Can it be charged with the BQ51010B component? As I can see, the output voltage options are around 4,2V.
1 - How the component can notice that the battery is completely charged at 3,7V?
2 - How the component will stop charging the battery?
3 - How the charging ending can be notified? I see that CHG can do that, but as long as I have test it, CHG is always high (both charging or not)
Thank you so much in advance,
Gerardo
Best Regards,
Bill Johns, Applications Engineer
Texas Instruments Inc
Dallas, Texas
For more information on Battery Charger Solutions see Link
Search "FAQ" on E2E Forum for common questions on battery charger solutions.
In reply to Bill Johns:
Excuse me, I made a mistake with the component name. The one I am using is BQ51050B.