Dear readers,
Every now ad then I need a negative power supply with a reasonable power. At ebay a and aliexpress the LM2576 positive output buck converters modules are sold cheap see fig1 and according schematic depicted in figure 2. Schematic 3 is an example of a buck converter with a negative power output coning from the TI LM2576 data sheets.
I examend the two schematics and looked for the differences. I noticed that basically only the negative lead of the input capacitor has a different position between the two schematics. In fig2 it is connected to the ground and in fig3 to the output. From a module perspective the changes are that the output has changed label from output to ground, and the ground has changed label to negative output. Physically nothing has changed much except for then negative lead of the input capacitor.
Q1: Since this is so deadly simple I wonder if I'm making a thinking mistake. Can someone confirm if my idea to convert these modules to negative output modules is correct or not ?
Q2: If it is correct then I do have and other question. Why is the output current of the negative schematic fig3 0.7 A and not 3 Amp as it is for the positive buck power supply?. Can that be boosted somehow?
Hopefully one of you reads this and can tell me what is right or wrong here.
Regards Oscar Goos.
Fig 1: Module for sale at ebay and aliexpress
Figure 2: Positive buck converter
Figure 3: Negative buck Converter