This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 208
Part Number: TL5001
Dear sir/madam,
I am currently using TL5001 for boost converter design. The input is 5V, output is 12V. The power level is around 12 W.
I use N-mos IRF8707 for the main switch. The inductor is 22uH.
Do I need external driver for the mosfet I used?
I don't know why there is no output signal from pin 1 and the Pin3 (comp) and Pin 4 (SCP) is always high ( around 2.4V) when it was powered.
Would you please help me address these problems?
Best regards
Mingxiao Li