Other Parts Discussed in Thread: BQ25895
Hi Team.
My client wants to design a system such as:
1) Normally, 12V voltage is input from the external(using adapter), and the battery is charged to 3.8V at this time.
2) When the external power is cut off, the voltage of the charged battery is stepped up and output at 5V / 1.5A for use in the internal system.
3) I would like to use the OTG function of BQ25890H to perform the above.
Can the BQ25890H perform these functions without any external control?
Please refer to the picture below