Other Parts Discussed in Thread: TPS3890, TPS3128, TPS3123
Hello,
We need a POR circuit with attached waveform for the CPU on our PCB. The CPU pin voltage is 1.8V.
Which part would you recommend? Maybe it should be something similar to Maxim MAX6898. I also found UC3903 that have more POR lines than needed, but the voltage level might be matching better...?
The LP3470 seems to be for higher voltages than the 1.8V CPU pin uses. Please advise.
If it still works, to achieve an about 3.8ms delay would you recommend 2nF capacitor on SRT-pin?
Thanks & regards,
-albin