Part Number: UCC27714
REFERENCE PAGE 23 -
"The circuit in Figure 49 shows a two-transistor forward converter circuit driven by the UCC27714. This circuit requires both outputs to be high or low simultaneously. The bootstrap capacitor would be charged with LO high state only (HO low). As this would decrease overall system efficiency two additional diode and two additional transistors are required to charge the bootstrap capacitor during LO and HO low period.)
QUESTION : (Figure 49. Two-Transistor Forward Converter Circuit) I SEE THE TWO ADDED SWITCHES FOR THE BOOTSTRAP, BUT ONLY ONE ADDED DIODE. WHERE IS THE PROPER PLACEMENT OF THE SECOND ADDED DIODE?