This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: LM5022 transformer design calculation sheet

Part Number: LM5022

Hi TI Guys:

I have a design as below:

input: 12VDC or 90~264Vac

output: 24V1.6A

PMP7760 is 30V~800V input, it is similar to my project parameter,

 could you share me the transformer design calculation or PMP7760’s transformer, thx

My E-ail:jack.deng@wtmec.com