Hello,
My customer is looking for 1.25V reference having <500us Turn-On Settling Time (to 0.1%) and considering MAX6023EBT12 because it’s Turn-On Settling Time (to 0.1%) is very fast, 30us.
The REF3312 datasheet says Turn-On Settling Time (to 0.1%) is 2ms at CL=10uF. And minimum capacitive load is 0.1uF. Can you say when CL=0.1uF, the Turn-On Settling Time (to 0.1%) would be 20us (2ms/100)?
Best regards,
K.Hirano