Other Parts Discussed in Thread: BQ24610
Hi team,
We are designing a battery operated device and we are planning to use a battery with 7.4V ,10AH battery .
And we have a requirement that it should be charged within 4 hours, DC Input voltage is 9V and device should use this supply voltage when plugged through adapter, and must not use the battery voltage and instead it should charge the battery.So we are planning to use BQ24753 battery charging IC. Will this IC be used, Please suggest ? If no please let me know the other option that is available?
Please suggest the suitable Battery Fuel Gauge IC also that will satisfy the above requirement specified(basically I2C interface is preferred)
End application is handheld HMI device
Regards,
Karthik