This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62095: TLV62095 IC heats and not sinking enough current

Part Number: TLV62095
Other Parts Discussed in Thread: TPS62095

Dear Sirs,

I am starting a new design with the TLV62095 converter and i am using the guidelines advised on the datasheet. The schematic part was set like the below image:

For the design of the PCB board it was followed (strictly) the recommended guide lines on the datasheet:

When i try to tie a higher load to converter's output the device is not sinking enough current. The circuit is regulating the calculated voltage but, it only works with small loads (less than 100mA). I cannot understand what's happening because all suggested advices were followed and everyting was built based on the information on the datasheet. It seems the IC is heating a lot and then enters in thermal shutdown.

Can you help me to solve this issue? Should i consider to use the TPS62095? Is there special thermal cosiderations that should be taken in consideration (which are not in the datasheet)?