I am designing a device that can be battery powered or USB powered. If I set the output of the TPS61032 to 4.8V and also connect +5volts from the USB cable to the same net, will something bad happen, like current flowing backward through the TPS61032 to try to charge the battery? In a non-synchronous boost converter, I know the diode would prevent backward current and the boost converter would stop switching because the output voltage would be higher than the 4.8 volts. But since this is a synchronous converter, I don't know what would happen. I would prefer to use this chip because of the higher efficiency, if it will work.
Thanks,
Dave G.