Other Parts Discussed in Thread: TINA-TI, ,
Tool/software: TINA-TI or Spice Models
Hi,
We used LM5116 in a synchronous buck controller and the solution is similar as TI evaluation board LM5116-12EVAL, the parameter as below: input voltage is 30-60VDC, output voltage is 12VDC,
Peak current is 5A and the work current is 2-3A;
Now we have some issue for LM5116:
1.We can't change the PWM duty cycle whether it is no-load or full load;
2.Our circuit efficiency is lower than 90% if it is no-load(the reference is 99%), what is the right efficiency?
3.If we increase of the L1 from 10uH to 22uH, the efficiency is increased larger than 90%.
The schematic diagram as attachment for your evaluating, thanks.