This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 259
Part Number: TPS62092
Hello,
The customer heard charge pump capacitor of TPS6209x is to have phase margin adjustment function. I don't think it correct but please let me confirm this.
Do we have a TPS6209x phase margin simulation data?
Best regards,
Toshihiro Watanabe
Hello Toshihiro-san,
It's my pleasure to support you.
Quoting the datasheet at section 8.3.10:
"The CP and CN pins must attach to an external 10 nF capacitor to complete a charge pump for the gate driver. This capacitor must be rated for the input voltage. It is not recommended to connect any other circuits to the CP or CN pins."
So the phase margin is not affected by the charge pump capacitor.
I don't have simulation data of the phase margin, but I can provide you a measurement. What are the customer's Vout, Vin and load conditions?
Thanks and best regards,
Emmanuel
All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).
____________________________________________________
TPSM82480 - Industry’s smallest 5.5Vin, 6A DC-DC MODULE with forced-PWM and VSEL option. Ideal for FPGA and processor power. Only 3.6x7.9x1.55mm! Order samples now!
In reply to Emmanuel Granatello:
In reply to Toshihiro Watanabe:
I have answered your question offline.
Could you please give us a feedback to close this post?