Other Parts Discussed in Thread: BQ40Z50-R2,
Hi all,
It's the first time for a customer to use BQ3060PWR. he has several questions:
- when set up BQ evaluation software, which spec can be regulated to control "charge" and "discharge"?
- in calibrate page, the result is 3 cells but in real circuit is 4 cells. cell 1+2+3 =12V; cell 1+2+3+4 equals to 12V too. however in real circuit, he measured 4 input pins, the results are: VC1=15.8V; VC2=12.1V;VC3=7.8V;VC4=3.9V. Could you tell me which spec is relevant to this result?
- in SBS page, why the data cannot be changed? how to change them?
Thank you!!