This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: Can it be used with Alkaline Primary Cells?

Part Number: BQ35100


My application will consist of the following:
2-4 cells of Alkaline batteries (Zinc + Mn02)
Operational range of 2.2V to 12V.

1) Can the BQ35100 be used with alkaline batteries?

2) Can it go up to 12V?
The datasheet states an absolute max rating of 5.5V but the demo kit user guide lists a Vbatt+ to Vbatt- of 32V.

3) Are there any TI products that would provide coulomb counting and possibly voltage measurement for an alkaline cell application?

Thanks!