I use this IC to output 250mA current to my load system, using the pin6 LOAD to drive the WIFI module under the control of pin4 CTRL, but I found when I activate the ctrl pin to output 3.3V to load,the load's 3.3V doesn't remain steady, Should I add the value of capacitance to improve this issue? I just use the TPS62742's reference design. a 10uF ceramic capacitance is placed near pin1 , there are another 22uF ceramic capacitance and 2.2uH power inductor in series with the PIN2 and PIN5.
but after I tune off the voltage to Load system, then the 3.3V voltage can remain steady. So what I should do just to add the value of the capacitance? But the datasheet tells us 10uF ceramic close to the 2.2uH inductor is sufficient for 400mA current output?