Hi
Our customer has following requirement.
Device : 14006X (Fsw=1.1MHz)
Vin: 13V-30V
Vout:12V
Iout:0.1A
We are considering following way to select inductance. Could you please review it?
1.
Supposing Iout=0.6A with Vin(max)=30V, Vout=12V and Kind=0.3.
2.
As a result, L=36uH can be obtained.
3.
If L=36uH, ripple current would be 0.18A.
4.
If ripple current is 0.18A, the device should operate in CCM even if Iout is required 0.1A.
5.
However, if Vin = 13V ripple current would be 23mA.
I concern for small ripple current and phase margin because of selecting 36uH.
Is this way reasonable for selecting inductance?
If it is not proper L, can you provide proper L?
BestRegards