This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62122: TIDA-00690: Unable to send BLE broadcast

Part Number: TPS62122
Other Parts Discussed in Thread: CC2650

Hi Giovanni,

I'm in the same situation. I just build the "Tida 00690" as described in application note.

I have connected the CC2650 launchpad Rev 1.3 with default FW. I have measured 1.8V pulse at the input of CC2650 lounchpad, it is around 36ms, but I can not see and BLE message.

The CC2650 launchpad works properly when is powered by a costant 1.8V , I can see BLE ADV message

Any suggestion?

Kind regards

Paolo G.