Hi
My customer will use TLV1117LV15.
But they use this device under Vin=5V, Vout=1.8V and Iout=0.1A and they could output Vout=1.8V.
Could theyr use this device this using method?
They use TLV1117LV15 to have to use their company's proven devices.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer will use TLV1117LV15.
But they use this device under Vin=5V, Vout=1.8V and Iout=0.1A and they could output Vout=1.8V.
Could theyr use this device this using method?
They use TLV1117LV15 to have to use their company's proven devices.
Hi Yokota,
TLV1117LV18 is the 1.8 V output version of the TLV1117LV family. This is essentially the same device as TLV1117LV15 with the only difference being the regulated output voltage due to a different internal resistor divider.
Since there is no external access to the FB node (the midpoint of the internal resistor divider), there is no way to force TLV1117LV15 to regulate at a higher output voltage than the 1.5 V output that it is designed to output. Please use TLV1117LV18 for this application.
Very Respectfully,
Ryan
Hi Ryan-san