I've just breadboarded this part and am seeing some behaviors I didn't expect. I'm hoping to get some feedback to let me know if what I'm seeing is normal?
- I've got a 3.3V battery connected to VBAT pin, fully charged. I've got a solar cell connected to VIN_DC putting out 1.5V. The voltage on the VSTOR pin appears to follow the VIN_DC pin. I get 0V on the VRDIV pin. Seems I should get 1.25V on this pin? Also, should the VSTOR voltage be the same as the VIN_DC voltage?
- If I have 0V on VIN_DC, I get 0V on VSTOR, even with 3.3V on VBAT. Is this normal? I was under the impression that if VIN_DC fell below 80mV, VSTOR would be connected to VBAT. If this is not true, and VSTOR goes to 0V when there is no light on the solar cells, wouldn't it make more sense to connect the system load directly to the battery, rather than the VSTOR pin?