Part Number: USB-TO-GPIO
Hello!
I connected the USB-TO-GPIO to my computer and an "Unknown Device" issue will appear.
And the green LED will not light up.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: USB-TO-GPIO
Hello!
I connected the USB-TO-GPIO to my computer and an "Unknown Device" issue will appear.
And the green LED will not light up.
Connect the Adapter first to your PC without connecting the ribbon cable to the target.
If that does not help disconnect and use a different USB connection on your PC.
Only after the green LED is on, then connect to target.
Regards,
Hi!Bolurian:
No device is currently connected, only USB is connected!
The situation is still the same, change the USB cable, change the USB slot, and change the computer.
And I have two USB-TO-GPIO that are all the same situation .
Thank you!
Hi!Bolurian:
well!
In fact, I found the real problem!This is USB-TO-GPIO EEPROM (24LC64)
The program inside has been deleted!I found a lot of similar situations using Google search and TI E2E search.
Now I have two solutions:
method 1.
Using an EEPROM ISP, first use the normal USB-TO-GPIO adapter
Back up EEPROM data before using EEPROM ISP Write data to the erased EEPROM to restore USB-TO-GPIO
normal.
Method 2.
Locate the TUSB3210 driver and download it (www.ti.com/.../sllc160)
Because your company's driver does not have a digital certificate, it must do so.
First disable the digital certificate (press "F8" when Windows starts).
Make the TUSB3210 driver work properly,Then use the USB-TO-GPIO firmware loader
(www.ti.com/.../sluc199)Update firmware to restore USB-TO-GPIO normal.
Thank you!