Hi,
I am wondering if the calculation below to calculate the Balance Time is correct.
If I use the Resistors on the Eval Board (100R and 105R) the I get a Balance time of approx. 16000 s/mAh per cell. This is assuming a duty cycle of 66% but there is nothing mentioned where this value comes from.
Please confirm that this is correct. if so, is there a way to speed the process up?
Thanks,
Fred