This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62084A: About PG & Discharge Resistance

Part Number: TLV62084A

Hello,

My Customer is considering about TLV62084A.

They have two question about internal value of IC.

Q1) 

In datasheets is written ' The PG terminal is an open drain output and is specified to sink typically up to 0.5 mA ' .

What is min and max value of the sink current (0.5mA typ) ?

Q2) 

What is min and max value of the internal resistance for output discharge ?

Regards,

Taichi Nakamura

  • Hi Taichi,

    I will check if this data is available, Could you explain why you need these data?

    What is the concerns in the application?

    Thanks

    Sabrina

  • Hi, Sabrina-san

    The reason is each of follows.

    ・PG pin
    They will calculate pull up resistor for drive to 0V .
    They plan to use TLV62084A at 1.8V, In this case , pull up resistor value is 3.8MΩ using 500μA.

    ・Discharge resistance
    They want to calculate the min to max of fall time of the discharge time.

    Regards
    Taichi Nakamura
  • Hello Taichi-san,

    I have a couple of suggestions related to the scope they want to achieve:

    -The PG pin configuration is of an active low side type with PU resistor. This means that it is not feasible to drive the PG pin exactly at 0V. To achieve this result, the customer needs a digital buffer to be cascaded to the PG pin (given that the pin driven by this buffer is at high impedance). I would suggest this one, available in several packages: 

    As a conclusion, the data on the PG pin is not useful to achieve what you said the customer wants.

    -Output Discharge resistance is a different topic, I understand the concerns of the customer and I think it would be good to transfer this conversation on a private channel. I will contact you directly with our E2E chat.

  • Hello, Emmanuel-san

    Thank you for your reply.
    I accept your request in E2E chat.

    Regards,
    Taichi Nakamura