Dears,
Can you recommended me a LDO, input 3.3-5.5V, adjustable output, output 3.3V, 3.6V, 3.8V, 4V, current needs 500mA, SOT23-5 package.
Thank you.
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Elsa,
We do not have any adjustable LDOs in the SOT23-5 package that meet your 500 mA current requirement; however, please consider the TLV755P and TLV757P which are fixed voltage families that accommodate some of your output voltages.
The highest rated output current for our adjustable LDOs in the SOT-23 package is 400 mA as can be seen here.
Very Respectfully,
Ryan