This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381A-Q1: Powering RM57L843 - Some Questions when using 24 V supply input

Part Number: TPS65381A-Q1
Other Parts Discussed in Thread: RM57L843, , TIDA-00548, TPS65381EVM, TPS62170

Hi,

I'd like to power a RM57L843 with a TPS65381A-Q1. I need to consider a +24VDC input.

I've noticed there is a lack of available reference designs for this configuration. I have found a few reference options:

1. RM46CNCD

2. TIDA-00548 (Which is a 4-20mA reference design + RM41)

3. SLVA830 (Power steering reference design).

4. TPS65381EVM

There are other designs available for powering TMS570 devices from the TPS65381

The RM57L843 needs 1.20V at 1350mA and therefore I have two options as I see it.

1. Implement an external FET connected to the TPS65381A-Q1 and manage the heat dissipation.

2. Implement an external buck controller, such as in TIDA-00548 and use its output as the 1.2V feedback into the TPS65381A-Q1.

I feel solution 1 is the easiest path, but I'm very concerned about thermal issues as I know the RM46CNCD boards have exhibited a fair amount of heat in the past. I can't find a webench option for TPS65381 so its difficult to check the performance.

Can anyone provide any suggestion or feedback to my points 1 or 2 above, and more-over is there a RM57L843 + TPS65381 reference design available?

Thanks

Stomp!

  • Hi,

    I have assigned your request to responsible Applications Engineer and we will get back to you as soon as possible.

    Regards,

    Murthy
  • Hi Stomp,

     

    Thank you for your question. 

     

    Indeed, thermal design considerations when using a 24V input supply is of most concern.  The TPS65381A-Q1 includes a pre-regulator from input to 6V and then downstream LDOs with integrated FETs for all regulators except VDD1.  VDD1 is used to generate the core voltage and is an LDO controller with external FET, but the sense pin can also be used to monitor the output from a DCDC when thermal and efficiency concerns require such an approach.   In some cases it may be necessary to provide a pre-regulation from 24V to an intermediate voltage such as 8 to 12V to spread the power dissipation. 

     

    Because you are using a RM57L843 needing 1.350A it will almost certainly require a DCDC for the core rail if you are using it at maximum capability for efficiency and thermal considerations. 

     

    TI Design TIDA-00548 uses the 6V pre-regulator rail as the supply for the DCDC, TPS62170.  This is acceptable as long as the total loading on VDD6 doesn't exceed its rated 1.3A output and from 24V the thermal design of the system can keep the TPS65381A-Q1 under the maximum specified junction temperature of 150C.  In some cases alternatives may be pre-regulate the voltage from 24V into the TPS65381A-Q1 or power the core rail DCDC from the 24V directly, but that may be a large challenge depending on the variance of the 24V input to ensure the ripple on a 1.2x V rail is low enough with such a high input to output voltage ratio and minimum on times of the DCDC.

     

    One other note, the core rail for the RM57L843 is 1.14V to 1.32V which is not a symmetrical range when the typical supply is 1.20V and the voltage monitoring from the TPS65381A-Q1 is symmetrical to the typical value.  Normally 1.23 V is chosen as typical with the TPS65381A-Q1 so the worst case the voltage monitoring would detect UV and OV are:  with VDD1 resistor divider for 1.23 V output, the VDD1_UV threshold will be between 1.1562 V and 1.2054 V (excluding tolerance of the resistors), VDD1_OV threshold will be between 1.2669 V and 1.3038 V (excluding tolerance of the resistors).  It is recommended to use 0.1% tolerance or better resistors. 

     

    There have been a couple of other E2E posts in the past showing alternative DCDC designs for the core rail to allow flexibility in where and how the power and thermal considerations are placed on the PCB.  I have re-attached it to this E2E. 

    8078.2017-02-03 TPS65381A-Q1 with External DCDC.pdf

     

    We have also posted a thermal estimator which includes power in the external diode for VDD6 pre-regulator and FET (when using VDD1 LDO controller).  I have re-attached it as well to help make power dissipation estimates for thermal design considerations.

     

    2016-10-12 TPS65381 Power Estimator Draft - E2E.xlsx

     

    Please let us know if you have further questions.

     

  • Hi Scott,

    Firstly thanks for such a complete and precise answer, I did not even consider the symmetrical tolerance issue!.

    I think the best solution for my situation is to use an additional device like the TPS57160 to supply the core of the RM57L843. At least this device will give me 60V input capability where the TPS62170 looks likes its only 17V capable.

    Thanks again for your help!.

    Cheers
    Stmp!