Other Parts Discussed in Thread: TPS2069C, TPS2051
Dear expert,
Basically i want to power on the BBB with 5V 2.5A
because i need 1.5A power on USB port
hence i decided to make custom BBB it will exactly same as current BBB with a slight difference
currently on BBB we have U8 (TPS2051) but i want to use TPS2069C so that my usb device gets a max current of 1.5A and by the way my usb device needs 1.5A so don't worry about it is crossing USB2.0 specification and so on. it is correct that my USB deice needs 5V 1.5A power for some reason
also if i change the FB7 (240-2384-1-ND) to (240-2393-1-ND)
my question is if i change
1. U8 (TPS2051) to TPS2069C http://www.ti.com/lit/ds/symlink/tps2061c.pdf
2. FB7 (240-2384-1-ND) to (240-2393-1-ND)
and use 5V 2.5A adapter
will my usb now get 1.5A current that it needs since footprint and the schematics around U8 is same or do i need to change schematics around U8
Regards