Other Parts Discussed in Thread: MC79L
Current using a LM79L05ACM to create a rail from a +24V input where Ground is connected to VIN (pin2,3,6,7) and +24V is connected to GND(pin5) and I'm getting around 19V(24-5) on the OUT (pin1). We would like to use the part in a higher temperature environment that 70°. Does a higher temperature specified part exist in the same function footprint? What is the impact on lifetime and performance if the device is run higher than the rated 70°C.