Hi
Could you please help me to check the customer's schematics?
And I appreciate if you give me feedback.
I can send you full file by email If you need more information, please tell me.
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you please help me to check the customer's schematics?
And I appreciate if you give me feedback.
I can send you full file by email If you need more information, please tell me.
BestRegards
Hello
Review of BQ24074 Circuit below:
1.) BAT pin, C3 recommend moving to BAT pin sided of R9
2.) ILIM 1180 ohms -- 1.31A, looks OK
3.) TMR 49.9k ohms -- 6.653hr, looks OK
4.) ISET 820 ohms -- 1.09A, looks OK
5.) EN1/low & EN2 /hi -- Input current set by R-ILIM, looks OK
6.) TS pin R10 -- no value listed, 0 ohm OK
7.) Value of battery Pack NTC not reviewed
Update:
8.) ITERM pin -- OK to Float for a termination current of 10% CC current.