I posted the same basic question much earlier today and do not see it listed.
The Lm34910C, in the situation where it receives leakage voltages at the SW and the Feedback pin, then refuses to start when Vin is applied.
Using a bench supply I confirmed that concurrent application of all system voltage allows the LM34910 to operate. However if the Vin is sequenced after the other voltages it does nothing.
Here is a list of the voltages vs. pins
with Vin applied. 'locked-up', no switching
1 2.30v SW
2 6.62v BST
3 0v Isense
4 0v Sgnd
5 0v RTN
6 1.153v FB
7 2.497v SS
8 1.569 Ron/SD
9 7.08v Vcc
10 12.61v Vin
Here are the voltages before applying Vin
1 2.293v
2 1.954v
3 0v
4 0v
5 0v
6 1.148v
7 0v
8 1.237v
9 0.809v
10 1.807v
Please consider this information and perhaps you can provide insight to the problem?
Thank you.
Jaye