Other Parts Discussed in Thread: CSD16321Q5, CSD16340Q3
Dear Specialists,
My customer is considering TPS40007 and CSD16321Q5.
He has a question, so I would be grateful if you could advise.
---
I am considering CSD16321Q5 instead of Si4866BD
Is there circuit using CSD16321Q5 with TPS40007 reference design or other field?
Due to the specification of the controller of 3.3 V -> 1.2 V , the worst case of Vgs becomes about 2.6 V.
At this time, I think that FET may not turn ON due to variations.
It is helpful to know such information.
DC/DC Converter spec
Vin:3.3V, Vout:1.2V Iout:3.2A
---
I appreciate your great help in advance.
Best regards,
Shinichi