Other Parts Discussed in Thread: GPCCHEM
Seeking clarification for the expected value in the Cell Terminate Voltage and Qmax Cell 0 registers.
We are using a battery pack design with 3 Li-ion cells in series. Should the values for these two registers be calculated on a per-cell basis, or for the pack in total?
For example, the voltage at which the pack is expected to fail is 9.6V - should the Cell Terminate Voltage register be set to 3200mV (9.6V / 3)?
The expected capacity of the battery pack is 4800mAh - should the Qmax Cell 0 register be set to 1600mAh (4800mAh / 3)?
Are there any other registers that expect a per-cell value, rather than a total pack value?