Other Parts Discussed in Thread: TPS51206
Hello team,
Lately we have encountered some problems with the TPS62080 device that seem to be pattern dependent as it is used to generate 0.6V for VTT. Specifically it is my suspicion the device was going into low power state when the pattern is mostly or all "1's". We have a minor reowork to the board that adds a load on the output (~1.65ohm) to keep the device from going into low power state. We have been working the device very hard with this rework to see if it fails but it has been solid.
We are looking to TI to confirm our simulation in TINA is correct as well advise if adding this load resistance is a problem.
webench_design_1364399_127.TSC