Dear Specialists,
My customer is considering Cboot of BQ24250 and has a question.
I would be grateful if you could advise.
---
I have a question about the external capacitor attached to the BOOT pin of BQ24250.
There is specification of 0.033 uF on data sheet P.7.
However, it is necessary to respond with different capacity due to recent shortage of capacitors.
I am thinking, when the configuration is 0.022 uF + 0.01 uF = 0.032 uF, there are some difference in capacity and number.
Is it possble to use?
Is there a possibility of affecting the operation?
---
I appreciate your great help in advance.
Best regards,
Shinichi