Hi again. Regarding your comment: "... Also be cautious of the construction and connection of references to the high current path, "ground" references can move substantially with short circuit..." it is ok to connect the GND to Earth (BAT-) with a net tie right? In the EVM pdf file, the net tie exists (7.2.3 page 44) so I used a net tie as well. In the file attached, the net tie is highlighted with a circle around it within the PDF and JPG files. This can not cause the problem (Microcontroller resets in the event of short circuit) right?
Thanks for your consideration.LFP.rar