Other Parts Discussed in Thread: TPS65910
Hello,
Regarding to ILMAX register on TPS65910AA1, my customer is asking some question.
They use 600MHz(@OPP100) on AM3554, currently ILMAX register of VDD_MPU is configured to 1.0A(ILMAX = 0).
(According to datasheet table 5-10, VDD_MPU current is 600mA(max) at OPP100.)
(Question)
1) When MPU clock is change to 800MHz(@turbo), should VDD_MPU current need to change to 1.6A(ILMAX = 1)?
Because it is 800mA(max) at turbo mode on datasheet table 5-10.
2) At EEPROM mode, is ILMAX register configured to default value(ILMAX = 0 :1.0A)?
Regards,
Tao_2199