Other Parts Discussed in Thread: BQ25703, , EV2400
Hello,
I am using bq25703a for the battery Charger. I manage to establish a communication between this module and the card STM32F4 .The communication is well established and I manage to write and read data in the registers of bq25703 but there are two registers I can not handle (the register 03 / 02h and the register 2D / 2A), in fact I can not write charge current in the register 03 / 02h (it is always at zero) and I can not read VBAT from 2D / 2C register.
NOTE: I am using the EVM BQ25703AEVM-732.
Is there a specific configuration to write to bq25703a registers before writing charge current or reading VBAT?