Hi,
I have a question regarding the "Load Disconnect During Shutdown" feature. Input voltage is 5V, output voltage is 3.3V. When i shut down the device Vin is 0V but the output voltage is still at 3.3V due to an external source. Can this voltage at the output during shutdown influence the input side of the converter?
Am i safe to assume that as long as EN is GND the input side can not be influenced by the output side?
"The device is put into operation when EN is set high. It is put into a shutdown mode when EN is set to GND. In shutdown mode, the regulator stops switching, all internal control circuitry is switched off, and the load is disconnected from the input."
Thank you!
BR,
Stefan