I tried with a series PFET (CSD23381F4T) with its source connected to VREF_SAMP, but as soon as the FET turns off, VREF_SAMP drops quickly to zero, probably because of the leakage through the FET. So then I tried with the ADG701 switch which advertises only 10 pA leakage current, but still could not hold the VREF_SAMP voltage constant (leaking slowly). Do you have any suggestion for a sample-and-hold with large hold time (5 seconds) for this situation? The key is probably extremely low leakage components.
Also, the bq25504 datasheet specifies a maximum limit of 11 nF for C_REF. Can you please tell me the reason?