This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/TPS7A4701-EP: Simulation with this device (along with the TPS7A4733) works with resistor loads, but the circuit stops working properly with a Balanced Line Receiver (THAT1200) as a load

Part Number: TPS7A4701-EP
Other Parts Discussed in Thread: TINA-TI, TPS7A33

Tool/software: TINA-TI or Spice Models

Hello,

I have built an LTSpice model (shown in the attached) for the TPS7A4700 and TPS7A33. When I add resistors, it functions well. Likewise the Balanced Line Receiver THAT 1200 works well too, when using voltage supplies provided in LTSpice. However, when I add the THAT 1200 Balanced line receiver, the circuit no long works. It appears to start out with a DC voltage on the output, which I think may be affecting the output regulation function.

Can you please have a look and see if you see any clues as to why this would happen?


Thanks in advance,
Cody



1200_test.zip