This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: The clamp P-MOS waveform isn't right when do the tests of UCC2897A low temperature

Part Number: UCC2897A

Hi team,

My customer is using the UCC2897A now. When they do low temperature test -30°C,the waveform is weird. The yellow is Vgs of P-MOS,green is the Vds of  P-Mos. The blue is VDD, the red is the Vss.

The weird waveform shows. When VCC trigger UVLO, the P-mos should be no drive signal. The drive voltage is 4~5V.

could you please help check the reason of the problem?

thanks.