Hello team,
Is there any risk if TLV1117LV works between the recommended maximum and absolute maximum input voltage?
The recommended maximum voltage is 5.5V, the absolute maximum voltage is 6V. However, in some condition, the input voltage will rise to 5.7V for 10min+.
"These are stress ratings only, which do not imply functional operation of the device at these or any other conditions beyond those indicated under Recommended
Operating Conditions" It's not easy to understand this description in the datasheet.
Thanks.
Dongbao