Hi Daniel,
In my prior question regarding "ESR requirement and stability" for this VTT regulator, you previously responded that the gm parameter is not tested to provide min/max characteristics in the electrical characteristics section. Furthermore you've also stated that all the cited values in the datasheet and excel calculator are typical values. There is variation of about 23% at 3A between those two resources (250S datasheet, 308S excel calculator ). In my analysis this variation is large enough to create problems for us at high loads across EOL tolerances without the RC filter. Is there a point of contact I can speak to regarding possibly screening these components for gm at various bias points? One way for us to address this would be to ensure that the gm of the parts we purchase is below a maximum limit.
Thanks,
John