Hello,
Input voltage may be changed from 2.8V to 3.8V. Output voltage is 3.3V. Load current is 1mA max.
Figure 5 of datasheet, VDO is almost 0V in condition. I think no issue if Vout is almost VIn condition is ok between 2.8V to 3.3V.
Please let me confirm if it is no issue or not. If no issue, how much is the max VDO approximately at 1mA load current?
Best regards.
Toshihiro Watanabe