Hello
I face recently failures of regulation with the LP2985, appeariing on some boards.
The LDO is fed by a 12V supply, not well regulated, with ripple at 1kHz.
See below the startup sequence
We see clearly that the LDO outpèut is not at 3.3V at startup (3.5V) and then goes up to 4.8V and then pump in regulation at 1kHz and not at all around an expected average of 3.3V.
This LDO clearly has a failure, and the lack of regulation affects also the 3V3 feeded microcontroller. Detroying permanentently the MCU, or the power stage (this board is used to regulate up to 10A / 150V)
Already checked:
1) Max LDO input unable to go higher than 14.8V (on failed boards, over the complete temperature range)
2) LDO output stability with 10uF 25V X7R cap: stable on a 20us 100mA overload pulse, each 1ms
3) At power off, output to input voltage not greater than 150mV
Do you have some advice for additional measurments to find the root cause?
Thanks
Christophe