Other Parts Discussed in Thread: TPS24700,
Hi,
The load is 12V and when the current go up to around 20A, both TPS24700 and TPS24701 got damaged, schematic is as below:
do you have any suggestion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zhao,
The design calculator is not entered correctly. please see below comments.
1. The SOA current values at Vin max that you entered are wrong. Please see below red line for correct values.
2. In your schematic, I see only one FET. In the Calculator you mentioned that you have 2 FET's. How many FET's do you have ?
3. In the design Calculator, you mentioned the start up load in 0.5 Ohms. With so much load, the system will not start. What is the actual load during start up? We generally recommend to start with no load.
4. Is your maximum Ambient temperature 25C or higher ?
Even with considering 25C ambient, 1K Start up Current, 2FET's (but correct SOA parameters) the SOA margin is -217%. This is not acceptable. The FET's will damage. We generally advice greater than +30% margin.
Also, during ouput Short Condition, the Source is pulled to GND. Now momentarily, +25V Gate voltage is applied across Vgs by controller. The FET Vgs is rated only for +/-20V. This condition can also damage the FET.
looks like there is no TVS clamp at the input. if there is a transient event and the controller turns OFF the FET, there will be high Positive Voltage generated across Vcc pin due to input inductance. Any voltage above 18V at Vcc, Sense can damage the device.
Please click "This resolved my issue" button if this post answers your question.
Regards,
Praveen