Hi,
Could you evaluate if the following connections made in protection FET of OUTx pin of LP8860 are suitable?
Best wishes,
,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you evaluate if the following connections made in protection FET of OUTx pin of LP8860 are suitable?
Best wishes,
,
Hi,
Instead of using SQW output to bias the gate of an N-channel protection MOSFET, and as 5V isn't available in my design, I used 3.3V connected to the gate of SI2392, an N-channel MOSFET with Vgs threshold smaller than 3 V.
My circuit is depicted below:
Si2392 safe operating area is:
I'd appreciate if you could check my design of the overvoltage protection for OUTx pins of LP8860, I am not sure if SI2392 is suitable for it.
Best wishes,
Hi,
The voltage on OUTx pins when current source of LP8860 is on is 1V (maximum). We are trying to avoid layout changes in our design as it is in ramp up phase, that is why we are trying to avoid using SQW pin.
Changing the voltage in SQ2398 gate to 4V, all 4 LED strings presented very similar luminosity, that is the condition we were looking for. As SI2392's Vgs(th) is lower than SQ2398's , I am optimistic that SI2392 will work well, but to be sure I have to wait one week more until this P/N arrives.
Best wishes,