Hi
I'm developing a motor controller using the ISO5452 as the gatedriver controling a SIC mosfet with a Ron of 0.03 ohm
I'm looking into how to decrease the current that the gatedriver shuts down on, the circuit looks like this:
diode with Vf of 1.3-2 V in series with a resistor R, following the design suggestion in the datasheet
To avoid a redesign I need a solution which either adds a diode with larger forward voltage or increases the resistor value R
I'm looking for a solution where the gate driver shuts down at approx 80 A, giving the following calculation
(9V- Vf-80*Ron)/500uA = [8900 10300] ohm for R
Is this calculation correct, can I just increase the resistor R or is there another way to achieve the short circuit protection?