Other Parts Discussed in Thread: LM25066
Hello TI,
We use LM25066A as a hotwap controller on 12V main power loop.
Sometimes we read ''01'' or ''03'' on 78h register after we performing short test on 12V_STBY rail.
After checking the definition of 78h register, we don't understand the DEFAULT status meaning.
If the description of the MEANING column is true, the bit status will be the default value, am I right?
If it is, the 78h reading in normal operating should be ''06'' but it shows ''01'' on GUI most.
Could you clarify what's the read back value of LM25066A 78h in normal operation?
BR.
Stan.