Hi Team,
a customer is dimensioning the TPS57140-Q1. They are using a TI spread sheet for the TPS54x family called 'TPS54x40 & TPS54x60 Current-Mode Step-Down Converter Design Calculator', which they already had and Webench.
System requirements are the following:
- Vin: 8-32V
- Vout: 6V
- Iout: 0.565A
The spreadsheet puts out a max frequency of 1480 kHz, Webench on the other hand only 652 kHz. Of course the higher one would be better because smaller inductors could be used. So a frequency of around 935 kHz would be the goal for that. Which tool should be trusted? Is it possible to use TPS57140-Q1 safely at 940 kHz?
Thank you and best regards,
Franz