This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A7200: TPS7A7200

Part Number: TPS7A7200
Other Parts Discussed in Thread: TPS7A83A

Hi,

I would like to use TPS7A7200 LDO in my board design and I have question regarding the Output voltage setting pins. 

Can I connect the 50mV, 100mV, 200mV, 400mV, 800mV, 1.6V Output voltage setting pins via 0 ohm 0402 resistors to GND (some of the 0 ohm resistors would be assembled and some not, so if there will be a need to change the Output voltage I could do so by different setting of the 0 ohm resistors?

I ask the question because some 0 ohm 0402 resistors can have 50 mΩ resistance, is this value of resistance is ok and it would not effect the output voltage accuracy?